Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
TI900 Silicone Based Thermally Conductive Insulators Slide 9

In summary, the TI900 range of thermally conductive insulators from T-Global has a high thermal conductivity, a high dielectric breakdown voltage and is used when the lowest possible thermal impedance is required. TI900 is available in several forms and can also be supplied as custom parts based on the end user requirements.

ed in a thickness of 0.12 mm.
PTM Published on: 2012-02-21