This section of the presentation will cover the Wide Frame assembly process for SOD128, known as PMDTM for Rohm. The PMDTM package using the Wide Frame method, will replace conventional DO-214AC, also known as PMDS or SMA. This table here summarizes the key differences between the two production methods. Compared to the PMDU Wide Frame changes, there are also physical dimensions and recommended land pattern changes. Similarly to PMDU changes, PMDTM will also have electro plating of the leads with 100% Tin, laser markings with 30 dots, and will be Halogen Free. The following slides will discuss all these differences in detail.