Maker.io main logo

Precise Timekeeping with Raspberry Pi Pico & DS3231 RTC

151

2026-02-03 | By Rinme Tom

License: General Public License Breadboards Jumper Wires Arduino

Introduction

Accurate timekeeping is a cornerstone of many embedded applications—whether it’s logging sensor data with timestamps, scheduling events, or powering automation systems. In this guide, you’ll learn how to interface a real-time clock with a Raspberry Pi Pico microcontroller using the I²C protocol and display time, date, and temperature on a 16×2 I²C LCD.

This project is ideal for makers, hobbyists, and engineers who want to add reliable timing capabilities to their Raspberry Pi Pico designs.

DS3231 Module

Why Use the Raspberry Pi Pico RTC for Timekeeping?

Standard RTC modules often drift over time due to temperature variations, making them unsuitable for precise timing applications. The DS3231, however, integrates a temperature-compensated crystal oscillator (TCXO) that continuously adjusts for temperature changes, delivering industry-grade accuracy and stability across environments.

Key Advantages

  • High Accuracy: ±2 ppm timekeeping with temperature compensation.

  • Battery Backup: Maintains accurate time during power loss via a CR2032 battery.

  • Low Power: Well-suited for battery-powered projects.

  • Integrated Sensors: Reads ambient temperature for display or control logic.

DS3231 pinout

Core Concepts and Protocols

Understanding I²C Communication

I²C (Inter-Integrated Circuit) is a two-wire bus (SDA and SCL) that enables the Pico to communicate with multiple peripherals using unique device addresses—0x68 for the DS3231 and usually 0x27 or 0x3F for the I²C LCD backpack. This simplifies wiring and expands system flexibility.

RTC Functionality

The DS3231 tracks time down to seconds and up to years, including leap year correction. It also provides a programmable square wave output and two alarms that can trigger GPIO events on the Pico.

Breadboard Connection

Wiring and Circuit Design

Connect the DS3231 and LCD to the Raspberry Pi Pico:

  • 3.3 V → VCC on all modules

  • GND → Ground common

  • GP4 (SDA) → SDA on RTC and LCD

  • GP5 (SCL) → SCL on RTC and LCD

This setup uses a shared I²C bus for both the RTC and display, reducing GPIO usage and wiring complexity.

Wiring Diagram

Software Setup

Libraries Needed

For Arduino IDE programming:

  • RTClib – to access DS3231 functions

  • LiquidCrystal_I2C – to drive the 16×2 display

These libraries handle I²C communication, date/time handling, and screen formatting.

Synchronizing Time

There are two common methods to set the RTC time on first use:

  1. Auto-sync from computer on upload – Saves the current compile time to the RTC.

  2. Manual date/time setting – Useful for scheduled demos or across multiple devices.

Sample Arduino Code

The example firmware initializes I²C, checks the RTC presence, and continually reads time and temperature for display:

Copy Code
#include <Wire.h>
#include "RTClib.h"
#include <LiquidCrystal_I2C.h>
#define DS3231_ADDR 0x68
#define LCD_ADDR 0x27

RTC_DS3231 rtc;
LiquidCrystal_I2C lcd(LCD_ADDR, 20, 4);

void setup() {
  Wire.begin();
  lcd.init();
  lcd.backlight();

  if (!rtc.begin()) {
    lcd.print("RTC NOT FOUND");
    while(true);
  }

  if (rtc.lostPower()) {
    rtc.adjust(DateTime(F(__DATE__), F(__TIME__)));
  }
}

void loop() {
  DateTime now = rtc.now();
  float temp = rtc.getTemperature();

  lcd.setCursor(0, 0);
  lcd.print("Time: ");
  lcd.print(now.hour());
  lcd.print(":");
  lcd.print(now.minute());
  lcd.print(":");
  lcd.print(now.second());

  lcd.setCursor(0, 1);
  lcd.print("Temp: ");
  lcd.print(temp);
  lcd.print(" C");

  delay(1000);
}

This code continuously updates the LCD without blocking main execution, keeping the UI responsive.

Troubleshooting & Tips

  • RTC Not Found: Check I²C wiring and module power.

  • Incorrect Time After Reset: Ensure backup battery is installed and oriented correctly.

  • LCD Issues: Confirm correct I²C address (scan with I²C scanner tool) and contrast settings.

Advanced Ideas Using the DS3231

Once you master basic integration, consider these enhancements:

  • Power-uptime scheduler using RTC alarms.

  • Temperature-logging data logger with SD card.

  • Automated timed actions like pet feeders or alarms.

Conclusion

Integrating the DS3231 RTC module with the Raspberry Pi Pico empowers your projects with accurate timekeeping and scheduling functionality. From simple clocks to event-driven automation systems, this guide helps you build a robust foundation and expand into intelligent embedded designs.

Mfr Part # SC0915
RASPBERRY PI PICO RP2040
Raspberry Pi
Mfr Part # SC0917
RASPBERRY PI PICO H RP2040
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.