LIS3DH Triple-Axis Accelerometer Breakout Datasheet by Adafruit Industries LLC

View All Related Products | Download PDF Datasheet
fr adafrull learning system
Adafruit LIS3DH Triple-Axis Accelerometer Breakout
Created by lady ada
Last updated on 2019-08-22 11:52:26 PM UTC
* adafruit learning system
Overview
The LIS3DH is a very popular low power triple-axis accelerometer. It's low-cost, but has just about every 'extra' you'd
want in an accelerometer:
Three axis sensing
±2g/±4g/±8g/±16g selectable scaling
Both I2C (2 possible addresses) and SPI interface options
Interrupt output
Multiple data rate options 1 Hz to 5Khz
As low as 2uA current draw (just the chip itself, not including any supporting circuitry)
Tap, Double-tap, orientation & freefall detection
3 additional ADC inputs you can read over I2C
We kept seeing this accelerometer in teardowns of commercial products and figured that if it's the most-commonly
used accelerometer, its worth having a breakout board!
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 3 of 27
>111 111111111“ 71 [771717711177117171] 1111111111111111111111111111111
This sensor communicates over I2C
or
SPI (our library code supports both) so you can share it with a bunch of other
sensors on the same I2C bus. There's an address selection pin so you can have two accelerometers share an I2C bus.
To get you going fast, we spun up a breakout board for this little guy. Since it's a 3V sensor, we add a low-dropout
3.3V regulator and level shifting circuitry on board. That means its perfectly safe for use with 3V or 5V power and logic.
It's fully assembled and tested. Comes with a bit of 0.1" standard header in case you want to use it with a breadboard
or perfboard. Two 2.5mm (0.1") mounting holes for easy attachment.
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 4 of 27
* adafruil learning system
Pinouts
The little chip in the middle of the PCB is the actual LIS3DH sensor that does all the motion sensing. We add all the
extra components you need to get started, and 'break out' all the other pins you may want to connect to onto the PCB.
For more details you can check out the schematics in the Downloads page.
Power Pins
The sensor on the breakout requires 3V power. Since many customers have 5V microcontrollers like Arduino, we
tossed a 3.3V regulator on the board. Its ultra-low dropout so you can power it from 3.3V-5V just fine.
Vin - this is the power pin. Since the chip uses 3 VDC, we have included a voltage regulator on board that will
take 3-5VDC and safely convert it down. To power the board, give it the same power as the logic level of your
microcontroller - e.g. for a 5V micro like Arduino, use 5V
3Vo - this is the 3.3V output from the voltage regulator, you can grab up to 100mA from this if you like
GND - common ground for power and logic
I2C Pins
SCL - I2C clock pin, connect to your microcontrollers I2C clock line. Has a 10K pullup already on it.
SDA - I2C data pin, connect to your microcontrollers I2C data line. Has a 10K pullup already on it.
To use I2C, keep the CS pin either disconnected or tied to a high (3-5V) logic level.
SDO - When in I2C mode, this pin can be used for address selection. When connected to GND or left open, the
address is 0x18 - it can also be connected to 3.3V to set the address to 0x19
SPI pins:
All pins going into the breakout have level shifting circuitry to make them 3-5V logic level safe. Use whatever logic
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 5 of 27
level is on Vin!
SCL - this is the SPI Clock pin, its an input to the chip
SDA - this is the Serial Data In / Master Out Slave In pin, for data sent from your processor to the LIS3DH
SDO - this is the Serial Data Out / Master In Slave Out pin, for data sent from the LIS3DH to your processor. It's
3.3V logic level out
CS - this is the Chip Select pin, drop it low to start an SPI transaction. Its an input to the chip
If you want to connect multiple LIS3DH's to one microcontroller, have them share the SDI, SDO and SCK pins. Then
assign each one a unique CS pin.
Other Pins
INT is the interrupt output pin. You can configure the interupt to trigger for various 'reasons' such as motion, tilt,
taps, data ready etc. This pin is 3.3V logic output.
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 6 of 27
I‘IIIH IIHHIHHHH IIII II!II|I III II II II II II II II II II II II II II II
Assembly
Prepare the header strip:
Cut/break the header strip into two pieces, one 3 pin
and one 8 pin. It will be easier to solder if you insert it
into a breadboard - long pins down
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 7 of 27
.u- an. un- fil- all on. 3- :v- ,,L1
Add the breakout board:
Place the breakout board over the pins so that the short
pins poke through the breakout pads
And Solder!
Be sure to solder all pins for reliable electrical contact.
We'll start with the main 8 pins for power & the I2C/SPI
interface.
(For tips on soldering, be sure to check out our Guide to
Excellent Soldering
(https://adafru.it/aTk)
).
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 8 of 27
u‘ - ‘ .. eta-.1“. L!" nu
If you want to have the board be more mechanically
stable, or want to use the ADC pins, solder in the 3 ADC
pads too
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 9 of 27
u 0 a I a I 3' :3 3' 3' ii ad 3. 3i 3i .5- ma. Ni. uni Nu. n53 X I I I I I
You're done! Check your solder joints visually and
continue onto the next steps
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 10 of 27
* adafruit learning system
Arduino
You can easily wire this breakout to any microcontroller, we'll be using an Arduino. For another kind of microcontroller,
as long as you have 4 available pins it is possible to 'bit-bang SPI' or you can use two I2C pins, but usually those pins
are fixed in hardware. Just check out the library, then port the code.
I2C Wiring
Use this wiring if you want to connect via I2C interface
Connect Vin to the power supply, 3-5V is fine. Use the same voltage that the microcontroller logic is based off of.
For most Arduinos, that is 5V
Connect GND to common power/data ground
Connect the SCL pin to the I2C clock SCL pin on your Arduino. On an UNO & '328 based Arduino, this is also
known as A5, on a Mega it is also known as digital 21 and on a Leonardo/Micro, digital 3
Connect the SDA pin to the I2C data SDA pin on your Arduino. On an UNO & '328 based Arduino, this is also
known as A4, on a Mega it is also known as digital 20 and on a Leonardo/Micro, digital 2
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 11 of 27
l , V iqhx dhcce
SPI Wiring
Since this is also an SPI-capable sensor, we can use hardware or 'software' SPI. To make wiring identical on all
Arduinos, we'll begin with 'software' SPI. The following pins should be used:
Connect Vin to the power supply, 3V or 5V is fine. Use the same voltage that the microcontroller logic is based
off of. For most Arduinos, that is 5V
Connect GND to common power/data ground
Connect the SCL (SCK) pin to Digital #13 but any pin can be used later
Connect the SDO pin to Digital #12 but any pin can be used later
Connect the SDA (SDI) pin to Digital #11 but any pin can be used later
Connect the CS pin Digital #10 but any pin can be used later
Later on, once we get it working, we can adjust the library to use hardware SPI if you desire, or change the pins to
other pins.
Note: Photo below incorrectly shows GND to 3Vo. The correct connection is GND to GND as listed above!
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 12 of 27
Download Adafruit_LIS3DH library
To begin reading sensor data, you will need to download Adafruit_LIS3DH from our github
repository (https://adafru.it/jzb). You can do that by visiting the github repo and manually downloading or, easier, just
click this button to download the zip
https://adafru.it/jzc
https://adafru.it/jzc
Rename the uncompressed folder Adafruit_LIS3DH and check that the Adafruit_LIS3DH folder contains
Adafruit_LIS3DH.cpp and Adafruit_LIS3DH.h
Place the Adafruit_LIS3DH library folder your
arduinosketchfolder
/libraries/ folder.
You may need to create the libraries subfolder if its your first library. Restart the IDE.
We also have a great tutorial on Arduino library installation at:
http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use (https://adafru.it/aYM)
Download Adafruit_Sensor
The LIS3DH library uses the Adafruit_Sensor support backend so that readings can be normalized between sensors.
You can grab Adafruit_Sensor from the github repo (https://adafru.it/aZm) or just click the button below.
https://adafru.it/cMO
https://adafru.it/cMO
Install it just like you did with the Adafruit_LIS3DH library above!
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 13 of 27
17 // 11c // :1.“an m as Ilmfmxcillsaml n: Wham! Wm'ILDGDE mummy WMLW mummm¢ Mimiufiim WMLISMIB mumsmm mummxzmo mmmmm Mammucm mam MafnflLmnMLlel El 3105!, usana_mso, LISSIIILCLKII vvvvvvvefivvvvv mm mm- nu; = m x: 7111 an Al I an x 435 ran an zgau ms 3551 3641: ms 3695 um um ‘nu 1 mu x 1112 x. mu x 1715 x mu 1 w m E] mm ~
Accelerometer Demo
Open up File->Examples->Adafruit_LIS3DH->acceldemo and upload to your Arduino wired up to the sensor
Depending on whether you are using I2C or SPI, change the pin names and comment or uncomment the following
lines.
Once uploaded to your Arduino, open up the serial console at 9600 baud speed to see data being printed out
// Used for software SPI
#define LIS3DH_CLK 13
#define LIS3DH_MISO 12
#define LIS3DH_MOSI 11
// Used for hardware & software SPI
#define LIS3DH_CS 10
// software SPI
//Adafruit_LIS3DH lis = Adafruit_LIS3DH(LIS3DH_CS, LIS3DH_MOSI, LIS3DH_MISO, LIS3DH_CLK);
// hardware SPI
//Adafruit_LIS3DH lis = Adafruit_LIS3DH(LIS3DH_CS);
// I2C
Adafruit_LIS3DH lis = Adafruit_LIS3DH();
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 14 of 27
rmn m-x 4.19 ./. 2 7.1.91 w“ 41,95 .h-z 70.71 .IN 7mm mm 1. n.1a mu mum: V sum-A .
Normally, sitting on a table, you'll see X and Y are close to 0 and Z will be about 1 g or ~9.8 m/s^2 because the
accelerometer is measuring the force of gravity!
You can also move around the board to measure your movements and also try tilting it to see how the gravity 'force'
appears at different axes.
Not that you'll see there's
two
sets of data!
Accelerometer ranges
Accelerometeres don't 'naturally' spit out a "meters per second squared" value. Instead, they give you a raw value. In
this sensor's case, its a number ranging from -32768 and 32767 (a full 16-bit range). Depending on the sensor range,
this number scales between the min and max of the range. E.g. if the accelerometer is set to +-2g then 32767 is +2g of
force, and -32768 is -2g. If the range is set to +-16g, then those two number correlate to +16g and -16g respectively. So
knowing the range is key to deciphering the data!
You can set, and get the range with:
In the first line, you can use LIS3DH_RANGE_2_G, LIS3DH_RANGE_4_G, LIS3DH_RANGE_8_G,
or LIS3DH_RANGE_16_G
When reading the range back from the sensor, 0 is ±2g, 1 is ±4g, 2 is ±8g and 3 is ±16g range
Raw data readings
You can get these raw readings by calling lis.read() which will take a snapshot at that moment in time. You can then
grab the x, y and z data by reading the signed 16-bit values from lis.x , lis.y and lis.z . When you are done with that
data, call read() again to get another snapshot.
Normalized readings
If you dont want to noodle around with range readings and scalings, you can use Adafruit_Sensor to do the
normalization for you. Its a nice way to have consistant readings betwixt multiple types of accelerometers.
Adafruit_Sensor uses event ( sensors_event_t ) objects to 'snapshot' the data:
lis.setRange(LIS3DH_RANGE_4_G); // 2, 4, 8 or 16 G!
Serial.print("Range = "); Serial.print(2 << lis.getRange());
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 15 of 27
oooulss = |:I[E mum: Luann up Test! . usann fauna! Inna: = 26 and: ammo (mu : zinglk and: um dam (mu : aim]: click cud: 42mm (mu : 51591: click um detected (0x641 damn click cud: 42mm (mu : .1591: click flick deceased (0x641 damn click Click magma (mu : sum: click flick deceased (ml) single click click menu (mall . mm: click cud: dtcecced (0x151: anal: click Em-
Once you've getEvent 'd the data, read it out from the event object with event.acceleration.x , event.acceleration.y
& event.acceleration.z
The key point is that those values are floating point, and are going to be in m/s No matter the range!
It's up to you whether you want the raw numbers or normalized data - there's times you want to keep it simple and
avoid floating point numbers, and other times you may want to avoid doing the math for force conversion.
Tap & Double tap detection
One of the neat extras in the LIS3DH is tap & double-tap detection. By tapping the accelerometer or the PCB or
something the PCB is attached to you can create a type of interface.
Open up the tapdemo demo to run it! It defaults to I2C so change to SPI if you're using that interface.
The tap detection works by looking for when one of the axes has an acceleration higher than a certain threshhold for
longer than a certain timelimit. The threshhold is in 'raw' values so you have to adjust it based on the scale/range
you've configured for the sensor:
Larger numbers are less sensitive, you'll really need to just tweak as necessary for your project.
You'll also have to turn on click detection. This will also se the INT pin to pulse high whenever a tap or double tap is
detected. If you turn on double tap detection it will still 'decode' single taps but the INT pin wont pulse on them.
/* Get a new sensor event */
sensors_event_t event;
lis.getEvent(&event);
2
// Adjust this number for the sensitivity of the 'click' force
// this strongly depend on the range! for 16G, try 5-10
// for 8G, try 10-20. for 4G try 20-40. for 2G try 40-80
#define CLICKTHRESHHOLD 80
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 16 of 27
Flguve 15‘ Slngle and douhle cllck recognlflun (a); — — M. (b); Flgure 15 Iiluslrates a slngle click event (a) and a double cllck eveni (b). The devlce is able in distinguish between (a) and (b) by changing the sailings oi ms TAF_CFG regislel irom single to double click recognition.
setClick can actually take many more arguments, the full list is:
The timelimit timelatency and timewindow are in units of "ODR" so if you change the sample frequency of the LIS3DH
you'll have to adjust these as necessary. The App note has way more details on this, with pretty graphs &
eveything! (https://adafru.it/jwf)
You can get the current click status register with lis.getClick() . Note that will return the raw 8-bit reg known as
LIS3DH_REG_CLICKSRC
Even though that register has 'axis' bits that theoretically tell you which axis the click is from, unless you bolt the
breakout to a huge thing like a table and thwack the table, any 'direct hits' to the sensor itself will register on any/all
axes because of the small scale.
Reading the 3 ADC pins
Finally, there are 3 extra 10-bit analog-digital-converter pins available. The details on these pins is scarce but we do
have code for reading data for them. This might be handy if you have a device without any ADC's
// 0 = turn off click detection & interrupt
// 1 = single click only interrupt output
// 2 = double click only interrupt output, detect single click
// Adjust threshhold, higher numbers are less sensitive
lis.setClick(2, CLICKTHRESHHOLD);
void setClick(uint8_t c, uint8_t clickthresh, uint8_t timelimit = 10, uint8_t timelatency = 20, uint8_t timewindow = 255);
While you can put 0-3.3V into the ADC pins, the valid reading range is only ~0.9V to 1.8V
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 17 of 27
42512 [1mm IV] 42512 [1mm .v; 42512 moo IV) 42512 [1mm IV) 42512 mm: IV) 42512 moo IV) 42512 mm: IV) 42592 [155: IV) 4532): [1576 IV) 4605: [157: IV) -s1n4 (141: IV) 23:2: 45:0 [um-u) 4021)) (1492 In 21):: 49:3 [1379 In 4952; (1153 In m. 3mm (1:09.11; 4224 (nag-w) 21):: 5553 (1273 .v; 4154 (um IV) ms: 1:2 (1:39 In -9116 m7: IV) ma: 45:6 [11-2 IV) —12n (1352 IV) Ma: 31:71 (1am) IV) 5952 (126! IV) mm: 5215 (1223 IV) 29“ (1a1nIV) mm: 1m: (1531 IV) 255 (1517 IV) mt: 4:416 nus-V) 716m) (1157 IV) 2m: 1921) (1324 IV) Anca: 5529 (15:12 IV) 1561); (1131 IV) nncz 1936 (1241 IV) mm: mm (12:11 II) 52512 (9m: IV) m: 1.355 (1152 IV) was: 51:55 (1251 IV) 52512 (9m: IV) m 15:24 (1155 IV) not: 575 (15:: IV) m2 m mm mu m. m m m mcz m
You can load the readadc demo sketch to start reading
I connected a trimpot from ground (left pin) to 3.3V (right pin) and conneted the wiper (center pin) to ADC1
For pins that don't have anything connected, such as ADC2 and ADC3 you'll notice the values flicker around a lot. If
you don't like this, just tie the pins to GND and it will keep the values 'steady'
The values of the ADC range from -32512 to 32512 but note that they correspond to ~1.8V to ~0.9V. You can map the
raw values to an approx voltage using
Which will convert the raw adc value into volt in units of millivolts
volt = map(adc, -32512, 32512, 1800, 900);
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 18 of 27
* adafruit learning system fmtzmg
Python &
CircuitPython
It's easy to use the LIS3DH sensor with Python or CircuitPython, and the Adafruit CircuitPython
LIS3DH (https://adafru.it/uBs) module. This module allows you to easily write Python code that reads acceleration from
the sensor.
You can use this sensor with any CircuitPython microcontroller board or with a computer that has GPIO and Python
thanks to Adafruit_Blinka, our CircuitPython-for-Python compatibility library (https://adafru.it/BSN).
CircuitPython Microcontroller Wiring
First wire up a LIS3DH to your board exactly as shown on the previous pages for Arduino. You can use either I2C or
SPI wiring, although it's recommended to use I2C for simplicity. Here's an example of wiring a Feather M0 to the
sensor with I2C:
Board 3V to sensor Vin
Board GND to sensor GND
Board SCL to sensor SCL
Board SDA to sensor SDA
Board D6 to sensor INT (or use any other free
digital I/O pin)
And an example of a Feather M0 wired with hardware SPI:
Board 3V to sensor Vin
Board GND to sensor GND
Board SCK to sensor SCL
Board MOSI to sensor SDA
Board MISO to sensor SDO
Board D5 to sensor CS (or use any other free
digital I/O pin)
Board D6 to sensor INT (or use any other free
digital I/O pin)
The INT pin is used for tap detection, if you aren't planning on using the tap detection capability, you can
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 19 of 27
pm ‘5 usec or ap 9 ac won,| you aren panning on USng we ap ec Ion capam I y, you can on... .00...
Python Computer Wiring
Since there's
dozens
of Linux computers/boards you can use we will show wiring for Raspberry Pi. For other platforms,
please visit the guide for CircuitPython on Linux to see whether your platform is supported (https://adafru.it/BSN).
Here's the Raspberry Pi wired with I2C:
Pi 3V3 to sensor Vin
Pi GND to sensor GND
Pi SCL to sensor SCL
Pi SDA to sensor SDA
Pi GPIO6 to sensor INT (or use any other free
digital I/O pin)
And an example on the Raspberry Pi 3 Model B wired with SPI:
Pi 3V3 to sensor Vin
Pi GND to sensor GND
Pi SCLK to sensor SCL
Pi MOSI to sensor SDA
Pi MISO to sensor SDO
Pi GPIO5 to sensor CS (or use any other free
digital I/O pin)
Pi GPIO6 to sensor INT (or use any other free
digital I/O pin)
CircuitPython Installation of LIS3DH Library
The INT pin is used for tap detection, if you aren't planning on using the tap detection capability, you can
leave that pin disconnected
The INT pin is used for tap detection, if you aren't planning on using the tap detection capability, you can
leave that pin disconnected
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 20 of 27
Next you'll need to install the Adafruit CircuitPython LIS3DH (https://adafru.it/uBs) library on your CircuitPython board.
First make sure you are running the latest version of Adafruit CircuitPython (https://adafru.it/tBa) for your board.
Next you'll need to install the necessary libraries to use the hardware--carefully follow the steps to find and install these
libraries from Adafruit's CircuitPython library bundle (https://adafru.it/zdx). For example the Circuit Playground Express
guide has a great page on how to install the library bundle (https://adafru.it/ABU) for both express and non-express
boards.
Remember for non-express boards like the Trinket M0, Gemma M0, and Feather/Metro M0 basic you'll need to
manually install the necessary libraries from the bundle:
adafruit_lis3dh.mpy
adafruit_bus_device
Before continuing make sure your board's lib folder or root filesystem has
the adafruit_lis3dh.mpy, and adafruit_bus_device files and folders copied over.
Next connect to the board's serial REPL (https://adafru.it/Awz) so you are at the CircuitPython >>> prompt.
Python Installation of LIS3DH Library
You'll need to install the Adafruit_Blinka library that provides the CircuitPython support in Python. This may also
require enabling I2C on your platform and verifying you are running Python 3. Since each platform is a little different,
and Linux changes often, please visit the CircuitPython on Linux guide to get your computer
ready (https://adafru.it/BSN)!
Once that's done, from your command line run the following command:
sudo pip3 install adafruit-circuitpython-lis3dh
If your default Python is version 3 you may need to run 'pip' instead. Just make sure you aren't trying to use
CircuitPython on Python 2.x, it isn't supported!
CircuitPython & Python Usage
To demonstrate the usage of the sensor we'll initialize it and read the acceleration from the board's Python REPL.
If you're using an I2C connection run the following code to import the necessary modules and initialize the I2C
connection with the sensor:
Or if you're using a SPI connection run this code instead to setup the SPI connection and sensor:
import time
import board
import digitalio
import busio
import adafruit_lis3dh
i2c = busio.I2C(board.SCL, board.SDA)
int1 = digitalio.DigitalInOut(board.D6) # Set this to the correct pin for the interrupt!
lis3dh = adafruit_lis3dh.LIS3DH_I2C(i2c, int1=int1)
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 21 of 27
Now you're ready to read values from the sensor using any of these properties:
acceleration - The x, y, z acceleration values returned in a 3-tuple and are in m / s ^ 2.
shake - Detect when the accelerometer is shaken.
tapped - Detect when the accelerometer is tapped.
For example, to print acceleration:
To use shake, we've set the optional shake_threshold=15 . The default is 30 , but lower numbers make it easier to get
the shake response. Try the following code. Enter it into the REPL and then shake the board.
To use tapped, you need to use lis3dh.set_tap to tell it whether to look for a single- (1) or double-tap ( 2), and
provide a threshold. We've chosen to look for a double tap ( 2) and set the threshold to 60 . Enter the following code
into the REPL and then tap the board twice.
import time
import board
import digitalio
import busio
import adafruit_lis3dh
spi = busio.SPI(board.SCK, board.MOSI, board.MISO)
cs = digitalio.DigitalInOut(board.D5) # Set to appropriate CS pin!
int1 = digitalio.DigitalInOut(board.D6) # Set to correct pin for interrupt!
lis3dh = adafruit_lis3dh.LIS3DH_SPI(spi, cs, int1=int1)
x, y, z = lis3dh.acceleration
print(x, y, z)
while True:
if lis3dh.shake(shake_threshold=15):
print("Shaken!")
lis3dh.set_tap(2, 60)
while True:
if lis3dh.tapped:
print("Tapped!")
time.sleep(0.01)
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 22 of 27
That's all there is to using the LIS3DH sensor with CircuitPython!
Full Example Code
import time
import board
import digitalio
import busio
import adafruit_lis3dh
# Hardware I2C setup. Use the CircuitPlayground built-in accelerometer if available;
# otherwise check I2C pins.
if hasattr(board, 'ACCELEROMETER_SCL'):
i2c = busio.I2C(board.ACCELEROMETER_SCL, board.ACCELEROMETER_SDA)
int1 = digitalio.DigitalInOut(board.ACCELEROMETER_INTERRUPT)
lis3dh = adafruit_lis3dh.LIS3DH_I2C(i2c, address=0x19, int1=int1)
else:
i2c = busio.I2C(board.SCL, board.SDA)
int1 = digitalio.DigitalInOut(board.D6) # Set to correct pin for interrupt!
lis3dh = adafruit_lis3dh.LIS3DH_I2C(i2c, int1=int1)
# Hardware SPI setup:
# spi = busio.SPI(board.SCK, board.MOSI, board.MISO)
# cs = digitalio.DigitalInOut(board.D5) # Set to correct CS pin!
# int1 = digitalio.DigitalInOut(board.D6) # Set to correct pin for interrupt!
# lis3dh = adafruit_lis3dh.LIS3DH_SPI(spi, cs, int1=int1)
#PyGamer I2C Setup:
#i2c = busio.I2C(board.SCL, board.SDA)
#int1 = digitalio.DigitalInOut(board.ACCELEROMETER_INTERRUPT)
#lis3dh = adafruit_lis3dh.LIS3DH_I2C(i2c, address=0x19, int1=int1)
# Set range of accelerometer (can be RANGE_2_G, RANGE_4_G, RANGE_8_G or RANGE_16_G).
lis3dh.range = adafruit_lis3dh.RANGE_2_G
# Loop forever printing accelerometer values
while True:
# Read accelerometer values (in m / s ^ 2). Returns a 3-tuple of x, y,
# z axis values. Divide them by 9.806 to convert to Gs.
x, y, z = [value / adafruit_lis3dh.STANDARD_GRAVITY for value in lis3dh.acceleration]
print("x = %0.3f G, y = %0.3f G, z = %0.3f G" % (x, y, z))
# Small delay to keep things responsive but give time for interrupt processing.
time.sleep(0.1)
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 23 of 27
* adafruit learning system
Python Docs
Python Docs (https://adafru.it/C6d)
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 24 of 27
* adafruit learning system m/vzm: Snpu: m manna: nuwuh mmms ‘ a 4 s
Downloads
Datasheets
LIS3DH datasheet (https://adafru.it/jwe)
LIS3DH app note (https://adafru.it/jwf)
ST design resources (https://adafru.it/mQc)
Fritzing object available in the Adafruit Fritzing Library (https://adafru.it/aP3)
EagleCAD PCB files on GitHub (https://adafru.it/quF)
Schematic
click to enlarge
Fabrication Print
Dimensions in inches
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 25 of 27
© Adafruit Industries https://learn.adafruit.com/adafruit-lis3dh-triple-axis-accelerometer-breakout Page 26 of 27
© Adafruit Industries Last Updated: 2019-08-22 11:52:26 PM UTC Page 27 of 27

Products related to this Datasheet

ADAFRUIT LIS3DH TRIPLE-AXIS ACCE